PRODUCT LIST
- Manufacturing
- Infrastructure
- Financial Services
- Education
- Computing Services
- Transportation
- Government and Public Sectors
- Retail
- Healthcare
Delta Ultron NT Series helps make Ripe Components more productive!

Background:
Ripe Component Technologies Private Limited is a multinational company manufacturer of Mobile Devices (Mobile Cases, Mobile Charger and Mobile Battery) accredited with ISO 9001:2008, exclusively working for Samsung India Electronic Limited and is the single source vendor in India.
With Delta spreading business across verticals catering to different applications, Delta once again surfaced as a partner of choice for Ripe Components in plastic molding applications, with first of its kind of installation at Greater Noida plant of Ripe Components. 5 million Samsung handsets are manufactured with seamless support of Delta UPS.
Challenge:
Plastic moldings are among the most demanding work environments in any industry. Equipment used in molding has to endure specific heat, chemical reactions and abrasion. Delta Ultron NT Series 20-4000kVA UPS stands up to these specific conditions, helping almost nil downtime and increase productivity. To ensure 99.9% uptime of Ripe Component’s productivity, Ultron NT has been installed at their plant which provides required reliability and efficiency. Initially other company proposed Hi-Pulse model UPS for the mentioned applications. At the end, Delta’s technical competency with solid application sight helped to get the project.
Solution:
Industrial application UPS needs to be rugged, suitable to operate in industrial environment. Manufacturers need UPS systems that are reliable and efficient which can support their critical loads and can work under extreme defying conditions. To meet the demand of Ripe Components, Delta offered Ultron NT Series three phase UPS which are available in range from 20kVA to 4000kVA. The Ultron NT series is a True Online double-conversion UPS featuring customized input / output configuration for various applications. Ultron NT Series UPS with in-buit isolation transformer acts as an electrical firewall between the incoming utility power and sensitive loads. With N+X parallel capability for redundancy or capacity expansion, it guarantees high availability and reliability for customer businesses.
The Ultron NT series offers continued and seamless protection for your equipment even under unbalanced loading conditions. The economy mode further improves efficiency by 4% to 7% and saves on operational cost.
For extremely critical loads (which cannot use utility input mains neutral), the inbuilt isolation transformer helps to generate a “freshly derived neutral” which is galvanically isolated from the input mains neutral. Thereby nullifying any input/ source electrical disturbances being reflected at the connected output critical loads on the UPS.
Result:
Delta has been associated with Ripe Component for over 6 years as “a single supplier” and has a strong installation base of Ultron NT close to about 4MVA installed for molding applications at their Noida and Greater Noida plants. Having good experience with Ultron NT, Ripe Component is also considering Delta products for their upcoming expansion and new projects.
“We are associated with Delta for past 6 years and Delta Ultron NT UPS systems are used for our molding machine applications. Reliable performance has made Delta UPS a standard accessory to our production facility. . Delta UPS performance & the after sales support has been excellent. The extra mile they walk to fulfill our needs even in odd hours has been very impressive for all these years” says Mr. Ramakant Mittal, Head- Operations, Ripe Components.
Delta’s strengths are quality, support, and providing clients with outstanding products and customized solutions at a competitive ROI and TCO. Based on this association, Delta looks forward to receiving more projects from the manufacturing sector. Supported by good customer insights in solid solution offering, Delta has established itself as the power behind the most competitive manufacturers.
Request A Quote |