PRODUCT LIST
Empower Your Data Center with Delta’s InfraSuite Manager
![](/media/images/other/technical-DCIM.jpg)
Today, DCIM is not just a datacenter monitoring solution. In addition to monitoring, it also provides management, planning and optimization features. Users' expectations for DCIM are no longer for basic functions such as energy consumption monitoring and sending notifications for equipment issues. Users expect that a DCIM solution should optimize the performance and life cycle management of data centers. An optimal DCIM solution includes four aspects: measurement, analysis, planning, and action. DCIM provides a holistic view to assist data center managers with continuous monitoring of energy efficiency so that the actual operational performance can be compared with the original design requirements. A DCIM solution helps managers identify the possibilities for reducing wasted energy and to continue to calibrate/optimize the entire system.
Delta provides consulting services and has helped cross-industry customers implement DCIM for different types of applications such as data center management, energy management, smart factories, and facility site monitoring. Client industries include: manufacturing, telecommunications, finance, education, government, healthcare, entertainment, energy, transportation, and enterprises.
Formosa Plastics Group (FPG) chooses Delta’s InfraSuite Manager to optimize data center operations
Formosa Plastics Group, a leading global petrochemical conglomerate, needed to build a new energy-efficient backbone enterprise data center. The newly-built 750 kW data center in New Taipei City supports FPG’s IT operations and data centers around the world. Long-term reliability, flexibility for future expansion, and energy efficiency are the customer’s top requirements for their data center. Delta provides a comprehensive solution that ensures high efficiency power management and cooling, and also includes Delta InfraSuite Manager for remote management of the entire infrastructure and PUE. Delta’s DCIM system offers IT managers real-time critical and comprehensive information for different layers of the data center. This system helps data centers achieve a lower PUE and up to 30% annual energy savings.
The leading bank in Taiwan implements Delta’s InfraSuite Manager with an access control system
The pivotal role that the banking sector plays in economic growth and stability, both at the national and individual levels, requires continuous and reliable services. Today’s banking services are not only provided in traditional ways such as bank branches or ATMs, but the intensive application of internet, call center banking, on-line banking and mobile banking are also popular and widely used by customers. IT-based financial services are highly reliant on solid infrastructure as the operation backbone. Each day, a huge amount of new data is generated, processed, acted upon, and stored. This makes data center management and optimization critical for the banking industry. The leading bank group in Taiwan chose Delta’s InfraSuite solution to safeguard their new data center. The power capacity of the data center is 3 MW, with around 500 racks allocated in different floors of the building.
Delta’s DCIM solution includes Operation Platform, PUE Energy, Capacity, and Asset modules for data center management. The bank has also integrated their DCIM with an access control system and security system to manage rack access privileges for the data center. Data centers that use DCIM to visualize and understand their actual capacity needs are able to significantly limit any costly downtime. DCIM can also help a company that is approaching the limits of its data center’s capacity to get the most from their currently available power and potentially defer large capital expenditures on new facilities.
About Delta – InfraSuite Manager
The 5G and AIoT trends bring more opportunity for data center development but also provide more challenges for data center management. The Delta InfraSuite Manager is a fully featured DCIM software solution that provides different modules to fulfill the requirements of different types of datacenters. With its intuitive BIM 3D interface, users can easily monitor the data center to achieve energy savings, optimization and high-efficiency operation.
|
Operation Platform: |
|
Asset Module: |
|
Capacity Module: |
|
Asset Inspection Module: |
|
Work Order Module: |
|
Incident Module: |
Implementing Delta’s InfraSuite Manager to extend the data center life cycle
Delta’s InfraSuite Manager is among the ranks of truly comprehensive DCIM solutions that are designed to cover all of the enterprise’s infrastructure management needs. InfraSuite Manager was designed with a modular structure to ease implementation and simplify later upgrades. It ensures reliability and safety for your data center. With it, you can prevent downtime of your data center operations and lower the total cost of ownership. Real time alarm notifications let IT managers provide timely solutions to data center issues. InfraSuite Manager delivers automation and visibility into the data center and increases the ease of management on a comprehensive platform, which can extend the data center’s life cycle.