PRODUCT LIST
Delta installs RoomCool at the WuXi Institute of Technology in China

With excellent product performance, service and highly efficient solutions, Delta has installed Delta InfraSuite Precision Cooling with the RoomCool HED3670 for the datacenter at the Wuxi Institute of Technology. The Wuxi Institute of Technology demanded the coefficient of performance (COP) of the cooling system to be greater than 3.0 and RoomCool HED3670 has a COP of 3.2. The HED3670 consists of an EC fan and dual refrigeration systems. The continuously viable inner and outer fans are 30% - 49% more efficient than conventional fans and enable the HED3670 to operate reliably and efficiently. Delta’s InfraSuite Precision Cooling solution was distinguished from its many competitors by its excellent products and services again.
견적의뢰 |